PKR39809-02

Current Operated Detection Elements

Phase Overcurrent

Phase overcurrent detection monitors the RMS current in each phase in order to detect single phase, phase to phase or three phase faults.

A phase detection pickup occurs when the measured current ≥ the Phase Fault Detect current x the Phase Pickup Multiplier.

The fault detect time is calculated based on the magnitude of the fault current as a multiple of the Phase Fault Detect setting.

The phase current values are updated every 5 ms and the fault detect time is continually being recalculated while the pickup is active.

Unless the fault resets, a fault detection will ensue.

Configuration options for Phase Overcurrent fault detection and reset are listed in the table below.

Table 69 Phase Overcurrent Fault Detect and Reset settings

Phase Overcurrent Fault Detect Settings

Range/Options

Resolution

Default

Fault Current

10...1260 A

1.0 A

200 A

Pickup Multiplier

1.0...10.0

0.1

1.0

Reset Threshold Multiplier

90...100%

1.0%

90%

Fault Reset Time

0...10000 ms

1 ms

50 ms

EF

The EF element is driven by the residual current that is the real-time vector sum of the three phase currents.

The residual or earth current is calculated by digitally summing the phase currents sampled every 5 ms.

Residual current = A phase current + B phase current + C phase current or Ie = Ia + Ib + Ic

NOTE: The Zero Sequence Current (Io) is defined as Io = (Ia + Ib + Ic) / 3. Therefore the Zero Sequence Current (Io) is one third of the residual or earth current.

An EF pickup occurs when the measured current ≥ the EF Detect current x the Earth Pickup Multiplier.

The fault detect time is calculated based on the magnitude of the fault current as a multiple of the EF Detect setting.

The earth current values are updated every 5 ms and the EF detect time is continually being recalculated while the pickup is active.

Unless the fault resets, a fault detection will ensue.

Configuration options for EF detection and reset are listed in the table below.

Table 70 EF Detect and Reset settings

EF Detect Settings

Range/Options

Resolution

Default

Fault Current

10...1260 A

1.0 A

40 A

Pickup Multiplier

1.0...10.0

0.1

1.0

Reset Threshold Multiplier

90...100%

1.0%

90%

Fault Reset Time

0...10000 ms

1 ms

50 ms

Sensitive EF (SEF)

The Sensitive EF elements are driven by measured residual current.

The residual current used for the SEF element is determined by measuring the current in the common connection between the three CT secondary currents on the PCOM board.

Residual current = A phase current + B phase current + C phase current or Ie = Ia + Ib + Ic

NOTE: The Zero Sequence Current (Io) is defined as Io = (Ia + Ib + Ic) / 3. Therefore the Zero Sequence Current (Io) is one third of the residual or earth current.

A sensitive EF pickup occurs when the measured current ≥ the SEF Fault Detect current x the SEF Pickup Multiplier.

The fault detect time is calculated based on the magnitude of the fault current as a multiple of the SEF Fault Detect setting.

The SEF current values are updated every 5 ms and the SEF fault detect time is continually being recalculated while the pickup is active.

Unless the fault resets, a fault detection will ensue.

Configuration options for SEF detection and reset are listed in the table below.

Table 71 SEF Detect and Reset settings

EF Detect Settings

Range/Options

Resolution

Default

Fault Current

1...80 A

1.0 A

4 A

Pickup Multiplier

1.0...10.0

0.1

1.0

Reset Threshold Multiplier

90...100%

1.0%

90%

Fault Reset Time

0...10000 ms

1 ms

50 ms

NPS

The NPS elements are driven by the NPS current (I2) which is calculated in real time by digitally summing the phase currents sampled every 5 ms and applying the Fortescue formula for sequence components.

I2 = (Ia + Ib phase shifted 240° + Ic phase shifted 120°) / 3

An NPS pickup occurs when the measured current ≥ the NPS Fault Detect current x the NPS Pickup Multiplier. The fault detect time is calculated based on the magnitude of the fault current as a multiple of the NPS Fault Detect setting.

The NPS current values are updated every 5 ms and the NPS fault detect time is continually being recalculated while the pickup is active.

Unless the fault resets, a fault detection will ensue.

Configuration options for NPS fault detection and reset are listed in the table below.

Table 72 NPS Detect and Reset settings

NPS Detect Settings

Range/Options

Resolution

Default

Fault Current

10...1260 A

1.0 A

40 A

Pickup Multiplier

1.0...10.0

0.1

1.0

Reset Threshold Multiplier

90...100%

1.0%

90%

Fault Reset Time

0...10000 ms

1 ms

50 ms

Fault Detect and Reset Configuration

The Fault Detect and Reset settings for Phase, Earth, SEF, and NPS detection elements can be configured in WSOS on the Global Settings page.

Figure 194
Fault Detection and Reset settings for Phase, Earth, SEF, and NPS elements

Broken Conductor

Open circuit faults due to broken conductors or mal operation of switchgear will not cause an increase in current and are not detected by standard over current protection.

This type of fault will cause an unbalance and produce NPS current.

The broken conductor algorithm is based on monitoring the relationship between NPS and PPS currents and is independent of load fluctuations.

Broken Conductor can only be used if it has been made available either through WSOS in Feature Selection.

Display > Configuration > Feature Selection > Detection

Or it can be made available on the operator interface.

If available it can be configured on the Broken Conductor page in the WSOS Protection menu.

Figure 195
AS Broken Conductor settings

or on the operator interface.

A description of these settings are shown in the table below:

Table 73 AS Broken Conductor settings

Broken Conductor Detection Settings

Setting

Description

Off/On

Turns the Broken Conductor Detection off or on.

Setting Ratio

The threshold at which the Broken Conductor detection element will pick up

Definite Time

The time after a pickup for a Fault Detection to be logged.

Reset Threshold Multiplier

This is the percentage of the Broken Conductor pickup value at which reset timing begins.

Reset Time

Reset time will start when the Inps/Ipps ratio drops below the Reset Threshold.

When the Reset Time expires, the fault will be reset.

Broken Conductor fault detection pickup will occur when the following conditions are present:

  • Broken Conductor is Available.

  • Broken Conductor Protection is On.

  • The real time Inps/Ipps ratio exceeds the configured Inps/Ipps Setting Ratio.

A Broken Conductor pickup will be recorded in the Event Log.

A pickup will start the fault detect timer and if the pickup persists for the Definite Time setting, a Broken Conductor fault detection will occur.

Fault Reset

A Broken Conductor pickup will reset if the Inps/Ipps ratio drops to the Reset Threshold for the Reset Time. The Reset Threshold is 90% of the Inps/Ipps ratio by default.

A Broken Conductor reset event will be recorded in the Event Log.

Configuration options for Broken Conductor fault detection and reset are listed in the table below.

Table 74 Broken Conductor Fault Detect and Reset settings

Broken Conductor Detect Settings

Range/Options

Resolution

Default

Setting Ratio

0.10...1.00 INPS/IPPS

0.01 INPS/IPPS

1.00 INPS/IPPS

Reset Threshold Multiplier

90...100%

1.0%

90%

Reset Time

0.00...100.00 s

0.01 s

0.05 s

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.