PKR39809-02

Appendix L.5 - Auto-Changeover Status Codes

Table 155 Auto Changeover Status Codes

Code

Operator Interface ACO Status

WSOS Auto-Changeover Status

17

Not Ready: ACO OFF

Not Ready: ACO OFF

20

Not Ready: Both suppl. same state

Not Ready: Both supplies are in the same state

25

Not Ready: Preferred and Backup supplies dead

Not Ready: Both Preferred and Backup supplies are dead

258

Not Ready: Master maintenance required

Not Ready: Master maintenance required

259

Not Ready: Master is in a protection lockout

Not Ready: Master is in a protection lockout

260

Not Ready: Master not ready to operate

Not Ready: Master is not ready to operate

261

Not Ready: Master tripped from a different source

Not Ready: Master was tripped from a different source

262

Not Ready: Master Work Tag applied

Not Ready: Master Work Tag applied

263

Not Ready: Master in Local Mode

Not Ready: Master is in Local Mode

264

Not Ready: Master communications not responding

Not Ready: Master is not responding to communications

265

Not Ready: Master not enabled

Not Ready: Master is not enabled

266

Not Ready: Master has no supply voltage

Not Ready: Master has no supply voltage

268

Not Ready: Master failed to Trip or Close

Not Ready: Master has failed to Trip or Close

269

Not Ready: Master live aft HV Check

Not Ready: Master Load Side bushing failed to go dead after High Voltage Check Time

270

Not Ready: Master waiting for communications

Not Ready: Master is waiting for communications

271

Not Ready: Master Trip or Close isolated

Not Ready: Master Trip or Close circuit is isolated

272

Not Ready: Master closed from different source

Not Ready: Master was closed from a different source

274

Not Ready: Master Load side not dead

Not Ready: Master Load side is not dead

277

Not Ready: Master aborted

Not Ready: Master aborted

279

Not Ready: Master prot seq in progress

Not Ready: Master protection sequence in progress

280

Not Ready: Master port in Local Mode

Not Ready: Master communication port is in local mode

514

Not Ready: Slave maintenance required

Not Ready: Slave maintenance required

515

Not Ready: Slave is in a prot lockout

Not Ready: Slave is in a protection lockout

516

Not Ready: Slave not ready to operate

Not Ready: Slave is not ready to operate

517

Not Ready: Slave tripped from a different source

Not Ready: Slave was tripped from a different source

518

Not Ready: Slave Work Tag applied

Not Ready: Slave Work Tag applied

519

Not Ready: Slave in Local Mode

Not Ready: Slave is in Local Mode

520

Not Ready: Slave comms not responding

Not Ready: Slave is not responding to communications

521

Not Ready: Slave not enabled

Not Ready: Slave is not enabled

522

Not Ready: Slave has no supply voltage

Not Ready: Slave has no supply voltage

524

Not Ready: Slave failed to Trip or Close

Not Ready: Slave has failed to Trip or Close

525

Not Ready: Slave live aft HV Check

Not Ready: Slave Load Side bushing failed to go dead after High Voltage Check Time

526

Not Ready: Slave waiting for comms

Not Ready: Slave is waiting for communications

527

Not Ready: Slave Trip or Close isolated

Not Ready: Slave Trip or Close circuit is isolated

528

Not Ready: Slave closed from diff src

Not Ready: Slave was closed from a different source

530

Not Ready: Slave Load side not dead

Not Ready: Slave Load side is not dead

533

Not Ready: Slave aborted

Not Ready: Slave aborted

535

Not Ready: Slave prot seq in progress

Not Ready: Slave protection sequence in progress

536

Not Ready: Slave port in Local Mode

Not Ready: Slave communication port is in local mode

1044

Waiting: Both suppl. same state

Waiting: Both supplies are in the same state

1282

Waiting: Master maintenance required

Waiting: Master maintenance required

1283

Waiting: Master is in a prot lockout

Waiting: Master is in a protection lockout

1284

Waiting: Master not ready to operate

Waiting: Master is not ready to operate

1285

Waiting: Master tripped from a different source

Waiting: Master was tripped from a different source

1286

Waiting: Master Work Tag applied

Waiting: Master Work Tag applied

1287

Waiting: Master in Local Mode

Waiting: Master is in Local Mode

1288

Waiting: Master comms not responding

Waiting: Master is not responding to communications

1289

Waiting: Master not enabled

Waiting: Master is not enabled

1290

Waiting: Master has no supply voltage

Waiting: Master has no supply voltage

1292

Waiting: Master failed to Trip or Close

Waiting: Master has failed to Trip or Close

1293

Waiting: Master live aft HV Check

Waiting: Master Load Side bushing failed to go dead after High Voltage Check Time

1294

Waiting: Master waiting for comms

Waiting: Master is waiting for communications

1295

Waiting: Master Trip or Close isolated

Waiting: Master Trip or Close circuit is isolated

1296

Waiting: Master closed from diff src

Waiting: Master was closed from a different source

1298

Waiting: Master Load side not dead

Waiting: Master Load side is not dead

1301

Waiting: Master aborted

Waiting: Master aborted

1303

Waiting: Master prot seq in progress

Waiting: Master protection sequence in progress

1304

Waiting: Master port in Local Mode

Waiting: Master communication port is in local mode

1538

Waiting: Slave maintenance required

Waiting: Slave maintenance required

1539

Waiting: Slave is in a prot lockout

Waiting: Slave is in a protection lockout

1540

Waiting: Slave not ready to operate

Waiting: Slave is not ready to operate

1541

Waiting: Slave tripped from a different source

Waiting: Slave tripped from a different source

1542

Waiting: Slave Work Tag applied

Waiting: Slave Work Tag applied

1543

Waiting: Slave in Local Mode

Waiting: Slave is in Local Mode

1544

Waiting: Slave comms not responding

Waiting: Slave is not responding to communications

1545

Waiting: Slave not enabled

Waiting: Slave is not enabled

1546

Waiting: Slave has no supply voltage

Waiting: Slave has no supply voltage

1548

Waiting: Slave failed to Trip or Close

Waiting: Slave has failed to Trip or Close

1549

Waiting: Slave live aft HV Check

Waiting: Slave Load Side bushing failed to go dead after High Voltage Check Time

1550

Waiting: Slave waiting for comms

Waiting: Slave is waiting for communications

1551

Waiting: Slave Trip or Close isolated

Waiting: Slave Trip or Close circuit is isolated

1552

Waiting: Slave closed from diff src

Waiting: Slave was closed from a different source

1554

Waiting: Slave Load side not dead

Waiting: Slave Load side is not dead

1557

Waiting: Slave aborted

Waiting: Slave aborted

1559

Waiting: Slave prot seq in progress

Waiting: Slave protection sequence in progress

1560

Waiting: Slave port in Local Mode

Waiting: Slave communication port is in local mode

2305

Running: Master is supplying the Load

Running: Master is supplying the Load

2561

Running: Master is supplying the Load

Running: Slave is supplying the Load

3083

Abort: One-Way CO executed

Abort: One-Way Changeover executed

3091

Abort: One-Way invalid state

Abort: One-Way is in invalid state

3092

Abort: Both suppl. same state

Abort: Both supplies are in the same state

3094

Abort: Manual CO executed

Abort: Manual CO was executed

3330

Abort: Master maintenance required

Abort: Master maintenance required

3331

Abort: Master is in a prot lockout

Abort: Master is in a protection lockout

3332

Abort: Master not ready to operate

Abort: Master is not ready to operate

3333

Abort: Master tripped from a different source

Abort: Master was tripped from a different source

3334

Abort: Master Work Tag applied

Abort: Master Work Tag applied

3335

Abort: Master in Local Mode

Abort: Master is in Local Mode

3336

Abort: Master comms not responding

Abort: Master is not responding to communications

3337

Abort: Master not enabled

Abort: Master is not enabled

3338

Abort: Master has no supply voltage

Abort: Master has no supply voltage

3340

Abort: Master failed to Trip or Close

Abort: Master has failed to Trip or Close

3341

Abort: Master live aft HV Check

Abort: Master Load Side bushing failed to go dead after High Voltage Check Time

3342

Abort: Master waiting for comms

Abort: Master is waiting for communications

3343

Abort: Master Trip or Close isolated

Abort: Master Trip or Close circuit is isolated

3344

Abort: Master closed from diff src

Abort: Master was closed from a different source

3346

Abort: Master Load side not dead

Abort: Master Load side is not dead

3349

Abort: Master aborted

Abort: Master aborted

3352

Abort: Master port in Local Mode

Abort: Master communication port is in local mode

3586

Abort: Slave maintenance required

Abort: Slave maintenance required

3587

Abort: Slave is in a prot lockout

Abort: Slave is in a protection lockout

3588

Abort: Slave not ready to operate

Abort: Slave is not ready to operate

3589

Abort: Slave tripped from a different source

Abort: Slave was tripped from a different source

3590

Abort: Slave Work Tag applied

Abort: Slave Work Tag applied

3591

Abort: Slave in Local Mode

Abort: Slave is in Local Mode

3592

Abort: Slave comms not responding

Abort: Slave is not responding to communications

3593

Abort: Slave not enabled

Abort: Slave is not enabled

3594

Abort: Slave has no supply voltage

Abort: Slave has no supply voltage

3596

Abort: Slave failed to Trip or Close

Abort: Slave has failed to Trip or Close

3597

Abort: Slave live aft HV Check

Abort: Slave Load Side bushing failed to go dead after High Voltage Check Time

3598

Abort: Slave waiting for comms

Abort: Slave is waiting for communications

3599

Abort: Slave Trip or Close isolated

Abort: Slave Trip or Close circuit is isolated

3600

Abort: Slave closed from diff src

Abort: Slave was closed from a different source

3602

Abort: Slave Load side not dead

Abort: Slave Load side is not dead

3605

Abort: Slave aborted

Abort: Slave aborted

3608

Abort: Slave port in Local Mode

Abort: Slave communication port is in local mode

3610

Abort: Slave detect seq in progress

Abort: Slave detection sequence in progress

3611

Abort: Slave is in a detect lockout

Abort: Slave is in a detection lockout

3612

Abort: Slave upstream lockout

Abort: Slave upstream device is in lockout

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.