PKR39809-02

Custom Menu

The custom menu is a user defined collection of standard PowerLogic ADVC Controller screens duplicated in a separate menu. It can be configured to only show those pages required for standard operation thus making the operation of the O.I. more user friendly. Up to 40 pages can be mapped to the custom menu.

The custom menu can only be configured through WSOS and the feature must firstly be made available in feature selection.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.