PKR39809-02

Battery Tray and Batteries

CAUTION
HAZARD OF FIRE
  • Only trained and authorized personnel who are familiar with the latest safety guidelines, technical documentation, and equipment labels must handle tasks such as installing, connecting, starting up, maintaining, or servicing battery systems.
  • Replace the battery with an equivalent battery to the original.
  • Use only the appropriate connectors to connect the battery.
  • Check the polarity before turning on power to this device.
  • Do not exceed the battery's operating temperature range, refer to Table 1 ULTRA versus COMPACT Power Supply Options for additional information, Ultra versus Compact Options).
Failure to follow these instructions can result in injury or equipment damage.

Figure 7
2 x 7.2 Ah Batteries on tray

Figure 7 shows two 7.2 Ah batteries mounted on the battery tray in the base of an PowerLogic ADVC Controller cubicle. They are attached by velcro straps.

The battery tray is made from stainless steel and shaped to restrict movement of the batteries. It is also mounted at an angle to make battery handling easier.

An EPDM rubber battery protector mat is placed on top of the tray and velcro straps are used to hold the batteries in place. The mat is designed to help protect the batteries and straps.

A battery temperature sensor is built into the battery tray. The sensor is used by the battery charging electronics to optimize battery life.

Figure 8
Battery tray temperature sensor

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.