PKR39809-02

Directional Protection Configuration

When Directional Protection is On, the active protection groups have duplicate directional protection settings. Changing a setting in one group, either forward or reverse, automatically changes that setting in the other group.

Some differences exist in the Global Settings for the two active groups. There are two settings that are common to both groups when Directional Protection is On.

  • Live Load Blocking

  • Sequence Reset Time

These settings are only displayed in the Global Settings for the forward protection group.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.