PKR39809-02

Example

In the example below, pressing the EVENT LOG key revealed that Auto Reclose was either turned on or off via WSOS and that Earth Protection was turned on via the OCP.

Possible event sources are shown in the table below:

Table 7 WSOS Event Sources

Source Explanation

WSOS

Windows Switchgear Operating System

OCP

OCP

PTCL

SCADA Protocol

IOEX

IOEX Card

NOTE: If a setting is changed via WSOS over Transmission Control Protocol/Internet Protocol (TCP/IP), then the first four characters of the user name, logged into the PC running WSOS, will be logged.

Sometimes the event log record for a setting change does not include enough information to identify the actual setting that was changed. For example, an event that reads Time Mult 1.00 identifies that a Time Multiplier setting for a particular protection curve was changed to 1.00. Pressing the EVENT LOG key when that setting change event was displayed may reveal for instance that it refers to the Group A, Trip 1 Phase Protection curve. (A:PH:T1)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.