PKR39809-02

Power Quality Tool Kit

Utilities are coming under increasing pressure from both customers and regulatory bodies alike to review the quality of power they are providing. This requires monitoring of the networks for various indices such as number of and duration of outages, sag/surge voltages and system harmonics.

The PowerLogic ADVC Controller takes advantage of the switchgear’s built in current and voltage sensors to provide power-monitoring abilities to meet the benchmark needs without the need for highly priced specialized monitoring instruments that require expensive additional current and voltage transformers.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.