PKR39809-02

Phase Rotation

The Phase Rotation setting is ABC by default. When the ACR or AS is installed in a network with ACB rotation this setting needs to be changed helps to ensure that the analogue measurements are reported correctly.

The Phase Rotation setting is also found in WSOS on the Status page.

Figure 111
Phase Rotation setting on the WSOS Status page

The Phase Rotation setting can also be found on the operator interface.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.