PKR39809-02

V0 Reset Threshold

If the measured zero sequence voltage value is less than the V0 Reset Threshold setting it will trigger a GFN reset condition.

NOTE: The Zero Sequence Voltage setting value must be carefully chosen considering the default system V0 prevailing in the network.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.