PKR39809-02

Trip and Close buttons

The Trip and Close buttons and the Trip and Close Disable lamps are configured separately. Therefore, there are four dialogues associated with customizing these functions.

Figure 55
Customize Trip and Close Keys

The Trip and Close dialogues can be used to:

  • Select the True/False colors for the lamps.

  • Determine if the status is displayed when the O.I. is off.

  • Determine if the button must be active when the O.I. is off.

  • Determine if the action must be delayed and what that delay must be.

The Trip and Close Disable dialogues can be used to:

  • Select the True/False colors for the Disabled lamps.

  • Determine if the status must be displayed when the O.I. is off.

All dialogues provide for comments to be added for later reference.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.