PKR39809-02

APGS Configuration

APGS is an additional protection feature that must be made available before it can be configured and enabled.

APGS can be made available through Feature Selection in WSOS:

Display > Configuration > Feature Selection > Protection

It can also be made available on the operator interface.

Once APGS is available it can be configured for a Change Time between 10 s and 180 s (default 60 s) and set to Auto.

In WSOS this is done on the Control page.

APGS Change Time and APGS Auto can be configured on the O.I.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.