PKR39809-02

Custom Menu Configuration

Configuration can be done on-line or it can be done in an off-line file and the Operator settings written to the controller when on-line.

Once the custom menu has been made available, the menu configuration dialogue box can be opened by selecting

Configuration > Menu Configuration in the Display menu.

This will open the Menu Configuration dialogue box below.

Figure 56
setVUE Menu Configuration pages

When the Edit button is pressed in the non-edit mode, the display changes to the edit mode allowing pages to be added and deleted.

In the Edit mode, the Edit button is replaced by Commit and Cancel buttons.

To add a page, click in a spare cell and choose a page from the drop down list.

To delete a page, select that page and press delete on the keyboard.

When the required custom menu pages are displayed, press Commit to make them active and return to the non-edit display.

The Rotation Time can also be configured on this page (rotational mode is explained below).

Figure 57
Custom Menu Configuration

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.