PKR39809-02

setVUE Quick Keys

The quick keys are provided to assist users not familiar with the menu structure on the setVUE O.I. to change commonly used settings more easily.

Controllers are shipped from the factory with default quick keys as shown but they can be configured individually for other functions if required.

Configuration of the quick keys using the setVUE O.I. was described in Configuring the Quick Keys. Refer to that section for more details. They can also be configured through WSOS which is explained here.

Firstly, quick key configuration must be made available through feature selection. When available, the quick key configuration page can be opened by selecting quick key configuration in the display menu.

The page in WSOS displays the quick keys in the same arrangement that they appear on the O.I.

Figure 46
Quick Key Arrangement

The fields on the WSOS quick key configuration page can be changed in the same way as any other setting. They can be changed directly when WSOS is on-line or they can be changed off-line and the new settings written to the controller.

A set of stick-on labels is provided with each controller to change the text on the quick keys to match the new function.

The functions available for quick key selection are:

  • Cold Load

  • Live Load Blocking

  • LOCAL/Remote

  • NPS Protection

  • Reset Flags

  • Work Tag

  • Battery Test

  • Reverse Cold Load

  • Auto On/Off

  • Earth Protection

  • Protection Group

  • Blank (no function)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.