PKR39809-02

Basic Current Protection Elements

The basic current operated protection elements in the PowerLogic ADVC Controller are:

  • Phase Over current

  • EF

  • SEF

  • NPS

NOTE: Phase Over current, EF and SEF protection are available by default but EF and SEF can be turned Off. NPS protection requires Sequence Components to be made available in Feature Selection before it can be used.

All circuit breakers used with the PowerLogic ADVC Controller as an ACR are fitted with 2000:1 (or a 1000:1 for the PMSet E Series) CTs on each phase. The CT secondary currents are continually sampled by the controller to detect over current faults on the system.

  • The Phase Over current element deals with the actual CT secondary values.

  • The EF element deals with the vector sum of the phase currents.

  • The SEF element deals with analogue measurement of the
    spill current < 80 A primary and uses a low pass frequency filter to remove harmonic content.

  • The NPS element deals with a value calculated in real time using the Fortescue formula for sequence components.

There is one global Trips to Lockout setting that applies to Phase Over current and EFs. SEF and NPS each have their own Trips to Lockout settings. They can also be set for between 1 and 4 trips but cannot exceed the global Trips to Lockout setting.

The global Trips to Lockout setting determines the maximum number of trips that can occur in a single sequence.

A sequence can end after less than the maximum number of trips if either the SEF or NPS Trips to Lockout settings is reached.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.