PKR39809-02

Activating Hit and Run

Once Hit and Run has been configured it can be activated by the operator at the Operator Settings 1 page in the System Status menu by selecting the Local/Remote control field (top left) and navigating to the Hit and Run On setting. See below:

When Hit and Run is turned ON the operator has a countdown period of 30 s (non-configurable) in which to press either TRIP or CLOSE, otherwise the setting will revert to the setting prior to turning Hit and Run ON.

While the 30 s non-configurable timer is running, the screen below is displayed.

Instead of waiting for the 30 s timer to expire, the operation can be aborted by pressing the SELECT key.

If the switchgear is closed and the operator presses the TRIP key, the following screen will be displayed and the countdown to operate will start to run:

The O.I. will beep every two seconds while the Hit and Run countdown is running. The beeping will become more rapid during the final 10 s.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.