PKR39809-02

UOV Close Blocking Configuration

For UOV Close Blocking to be used it must be made available.

It can only be made available through Feature Selection in WSOS:

Display > Configuration > Feature Selection

Once UOV Close Blocking has been made available it can be selected in WSOS on the UOV Protection page in the Protection Group settings.

Figure 173
WSOS UOV Close Blocking setting

NOTE: Selecting UOV Close Blocking will only affect the Close Blocking capability of that element. It will not impinge upon any other functionality that can effect a Close Block such as Loop Automation, Auto Reclose Block or Voltage Blocked Auto Reclose

Changes to the UOV Close Blocking On/Off status are recorded in the Event Log.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.