PKR39809-02

Changing Settings

If any protection settings, or settings from the following list change during a UOV protection sequence, the sequence will be aborted. If the switchgear was tripped due to UOV protection the ACR will go to Lockout.

  • Power Direction (Source/Load designation)

  • Protection On/Off

  • UOV Protection Available

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.