PKR39809-02

Using Delayed Operation

When active, Delayed Operation is the default action for the TRIP and/or CLOSE keys. So, if Delayed Operation has been configured for the controller, the local operator has no option other than to use it. However, if it is not required it can be bypassed as explained below.

To trip/close the switchgear after a pre-set interval.

  • Press the TRIP or CLOSE key.

The flexVUE screen will display the message below:
or

The displayed time will count down and the CAPE will beep every 2 s while the timer is running. The beeping will become more rapid during the final 10 s.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.