PKR39809-02

Custom Menu

The custom menu makes the O.I. easier to use by only displaying the pages that are relevant to operators performing basic functions.

In order to use the custom menu, it must have previously been configured through WSOS which is explained in setVUE Custom Menu.

If custom menus have been configured, an operator can access them by pressing the custom menu key.

Continuing to press the custom menu key will cause the display to scroll through the pages that are configured. Alternatively, the display may have been configured to scroll automatically when the O.I. is on.

The display can be returned to the normal menu by pressing the Menu key.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.