PKR39809-02

Current Measurement

All compatible switchgear suitable for use with the PowerLogic ADVC Controller are fitted with 2000:1 CTs in each phase. Details of the Current Transformers can be found in the Technical Specifications.

Phase and Earth current values are displayed as a Magnitude and Angle where:

  • Magnitude is the real-time RMS value.

  • Angle is the current angle relative to the corresponding phase to earth voltage angle.

NOTE: Earth current angle is the current angle relative to the zero sequence voltage angle.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.