PKR39809-02

Critical Settings

The load side is as defined by the Power Direction setting

And energized is as defined by the Live Line Threshold setting:

Which is configurable between 2000 V and 15000 V in 1 Volt steps.

Both of these critical settings can be configured in WSOS on the Measurement page:

Display > Measurement

The Power Direction and Live Line Threshold settings can also be configured on the O.I.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.