PKR39809-02

APGS Applications

Sometimes an ACR is used at a location in a supply network where the power flow can be in either direction depending on the configuration of the network.

One example of this is a network tie point where the operator may have to select a different group of protection settings to compensate for a change in power flow when changing the network configuration.

Emergency switching configurations may require more than one protection group.

APGS is utilized by the Loop Automation function to change the active protection group during system reconfiguration.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.