PKR39809-02

Appendix K.8 ­ setVUE AS System Status Pages

This appendix shows all of the System Status display group pages and list display options and setting ranges.

The System Status display group contains the operator settings and information relating to the ratings and configuration of the device.

The basic System Status display group consists of 16 default pages.

Up to 19 additional pages (shown below in blue) can be added depending on the features that have been enabled.

Table 147 setVUE System Status Menu Pages for AS

System Status Menu

Default pages

Additional pages

Fault Flags/Pickup Flags

Supply Interrupt Flags(1)

Options – Detection 1(2)

Operator Settings 1

Options – Detection 2(2)

Operator Settings 2

Options – Detection 3(2)

Operator Settings 3

Options – Automation 2(2)

Operator Settings 4(1)

Options – Controller 1(2)

System Settings 1

Options – Controller 2(2)

System Settings 2

Options – Communications 1(2)

Switchgear Status

Options – Communications 2(2)

Fault Information

Options – Power Quality(2)

Live/Dead Indication

Quick Key Selection(3)

Phase Voltage and Power Flow

IOEX – A Status(4)

Terminal Designation/Rotation

IOEX – B Status(5)

Radio

Hit and Run(5)

Switchgear Type and Ratings

Waveform Capture(6)

Switchgear Wear/General Details

Waveform Trigger(6)

Plant Details(7)

Battery Test(8)

 

User Defined Control 1

User Defined Control 2

(1) Per Element Detection available.

(2) Panel display options available.

(3) Quick key configuration available.

(4) IOEX available.

(5) Hit and Run available.

(6) Waveform capture available.

(7) Plant Details Available.

(8) Battery health test available.

The top line of each page is the page title. To the right of the title is the letter S which indicates that the page being displayed is part of the System Status display group.

The next three lines are the data on display. Most displays have six data fields. The standard layout is shown below.

Where details of individual pages are shown below a small column has been added to the right of each field to indicate the type of data displayed. The letters in this column have significance as follows:

O Operator Controlled

D Display Only (that is cannot be changed)

P Password Protected (that is cannot be changed unless the password is entered)

R Operator Controller Reset (that is resets a field or group of fields)

If the standard menu is running the System Status menu will be displayed when the Panel On key is pressed.

The first page to be displayed in the System Status menu is the Fault Flags page shown below.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.