PKR39809-02

LOP Protection Summary

  • LOP protection operates on the loss of one or two phases but not three.

  • LOP Protection requires two settings:

    • LOP Voltage (2000...15,000 V)

    • LOP Timeout (0.1...100.0 s)

  • LOP protection can be set for:

    • Off

    • Trip

    • Alarm

Table 59 LOP Protection Settings/Specifications

LOP Protection Settings/Specifications

LOP Voltage range

2...15 kV Default 10 kV

LOP Voltage setting resolution

1 V

LOP Voltage accuracy(1)

2.5% ± 25 V

LOP Timeout range

0.1...100.0 s Default 10.0 s

LOP Timeout resolution

0.1 s

LOP Time accuracy

± 50 ms

(1) Includes accuracy of VTs in the switchgear.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.