PKR39809-02

Display Settings Units

Setting units can be displayed in either Imperial or Metric for example, gas pressure can be displayed in either kPag or psig.

Other settings that will be affected by a change of setting units include Distance to Fault measurements.

The Setting Units displayed can be changed from either the O.I. or WSOS.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.