PKR39809-02

LA Display

Once LA has been made available it can be configured in WSOS by going to:

Display > LA > Display.

The LA display page opens with Classic logic and Tie device type selected by default.

Figure 236
Default Classic LA WSOS display page

Changing the Logic setting to Intelligent changes the display page as shown below.

Figure 237
Default Intelligent LA WSOS display page

LA can also be configured on the operator interface.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.