PKR39809-02

Time Zone and Daylight Saving Configuration

Once Time Zone has been made available, Time Zone and Daylight Saving settings can be configured on the configuration setting page in WSOS by going to:

Display > Configuration > Time Zone and NTP Configuration.

There is also an option on this page to select SCADA master station time synchronization using Universal Time Coordinated (UTC) instead of local time.

Figure 44
Time Zone and NTP Configuration settings

NOTE: Time Zone and Daylight savings settings can only be configured via WSOS. These are not available for configuring via either of the O.I.s.

The below table describes the settings associated with Time Zone and Daylight Saving configuration.

Table 10 Time Zone and Daylight Saving Configuration settings

Setting Description

Time Zone

The time zone where the PowerLogic ADVC Controller is located.

Positive values are ahead of UTC

Negative values are behind UTC

Offset

Any offset from the standard time zone value.

Daylight Saving

Daylight Saving On

Select this to enable time adjustments due to daylight saving.

Time Zone

The time zone for when daylight saving is active.

Offset

Any offset from the daylight saving time zone value.

Start Month

The month when daylight saving will start.

Start Week

The week within the start month when daylight saving will start.

Start Day

The day of the week within the start week when daylight saving will start.

Start Time

The time on the start day when daylight saving will start.

Stop Month

The month when daylight saving will stop.

Stop Week

The week within the stop month when daylight saving will stop.

Stop Day

The day of the week within the stop week when daylight saving will stop.

Stop Time

The time on the stop day when daylight saving will stop.

Apply Button

When any value is changed in the time zone or daylight saving sections, the Apply button is enabled. This button must be selected for changes to be saved, otherwise the changes will be lost.

SCADA Time Synchronized using UTC

When this tick box is selected, SCADA synchronizes the PowerLogic ADVC Controller’s time using UTC. When it is not selected, SCADA synchronizes the PowerLogic ADVC Controller’s time using local time.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.