PKR39809-02

PSM

Figure 6
PSM

The PSM supplies power to the CAPE, and controls the supply from external auxiliary sources.

The PSM encloses all 115/230 Vac mains connections. Internally it provides terminals for auxiliary power supply connection. Cable-tie points are provided to attach the auxiliary supply cables. Miniature circuit breakers are used to help protect and switch the battery and auxiliary power supplies on/off. A durable cover is used to enclose all the terminations.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Only qualified personnel, trained, authorized, and familiar with the contents of the latest issue of the safety guide, safety information, technical data chapters, and the equipment rating labels shall work on installation, connection, commissioning, maintenance, or servicing of the equipment.
Failure to follow these instructions will result in death or serious injury.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.