PKR39809-02

Feature Selection

Feature Selection refers to the ability to make PowerLogic ADVC Controller features Available or Not Available as well as Allowing or Not Allowing selected functions.

Making a feature Not Available not only disables the features logic but also removes all reference to the feature in WSOS and on the O.I. The complexity of the user interface is therefore reduced as only the features in use are displayed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.