PKR39809-02

Dead Lockout on PMSet U Series

Dead Lockout cannot be turned On if the source side voltages are unavailable.

Therefore an ACR with PMSet U Series switchgear that does not have voltage sensing on the X side cannot use Dead Lockout if the X side is the designated Source.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.