PKR39809-02

Local Mode

In this mode, only a local operator can manually close the switchgear. (An ACR can still close automatically with the auto-reclose function during a protection sequence or due to an automatic feature such as loop automation if enabled.)

This means that an operator can go to the PowerLogic ADVC Controller, set local control mode and know that remote closing is disabled.

Only a local operator can apply or remove the work tag when the PowerLogic ADVC Controller is in local mode.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.