PKR39809-02

CLP Status

The current status of the CLP is displayed by WSOS on the Control page.

The Status is read-only and can be either Off, On or Idle.

Off – means that the feature is off and will have no effect on the protection settings.

On – means that at least one of the CLP protection elements is on and the displayed Multiplier is being applied to the Setting Current for that elements.

Idle – means that the feature is on but not currently affecting the protection settings.

Time – is the Operational Cold Load Time. Note this field is configurable.

Multiplier – is the current OCLM and is read-only.

The CLP Status is also displayed on the operator interface.

CLP cannot be turned On or Off via the Status display. That can only be done by selecting/deselecting one of the protection elements in the CLP protection settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.