PKR39809-02

Appendix P.1 ­ Analogue Points to Monitor and Set Pick-up Thresholds for Overcurrent Protection

New SCADA Analogue input and control points have been made available to allow users to view and alter pick-up thresholds remotely (via SCADA) for both the Active Forward and Reverse Phase, Earth, SEF, and NPS elements. In addition, a further Analogue input and control point is provided for the Active Broken Conductor Pick-up threshold (ratio of Inps/Ipps).

NOTE: The table below outlines the database points available Protection State Analogues and Protection Analog Controls features. For more details refer the N00-331 Database.

Table 159 New Protection State Analogues

Appendix/Sub Appendix

Point

Name

Description

Min

Max

Unit (s)

Res.

Dead band

Version Introduced

A2.5

5

Phase Setting Current Active

The Phase setting current of the active protection group

3

1260

Amps

1

1

50—14.70

A2.5

6

Earth Setting Current Active

The Earth setting current of the active protection group

3

1260

Amps

1

1

50—14.70

A2.5

7

SEF Setting Current Active

The SEF setting current of the active protection group

1

80

Amps

1

1

50—14.70

A2.5

8

NPS Setting Current Active

The NPS setting current of the active protection group

1

1260

Amps

1

1

50—14.70

A2.5

9

Broken Conductor Setting Ratio

The Broken Conductor setting current of the active protection group

10

100

N/A

0.—01

1

50—14.70

A2.5

10

Phase Setting Current Reverse

The Phase setting current of the active protection group

3

1260

Amps

1

1

50—14.70

A2.5

11

Earth Setting Current Reverse

The Earth setting current of the active protection group

3

1260

Amps

1

1

50—14.70

A2.5

12

SEF Setting Current Reverse

The SEF setting current of the active protection group

1

80

Amps

1

1

50—14.70

A2.5

13

NPS Setting Current Reverse

The NPS setting current of the active protection group

1

1260

Amps

1

1

50—14.70

Table 160 New Protection Analog Controls

Appendix/Sub Appendix

Point

Name

Description

Min

Max

Unit (s)

Res.

Version Introduced

B.2

40

Phase Setting Current Active

This controls the Phase Setting Current for the Active Protection/Detection group

3

1260

Amps

1

50—14.70

B.2

41

Earth Setting Current Active

This controls the Earth Setting Current for the Active Protection/Detection group

3

1260

Amps

1

50—14.70

B.2

42

SEF Setting Current Active

This controls the SEF Setting Current for the Active Protection/Detection group

3

1260

Amps

1

50—14.70

B.2

43

NPS Setting Current Active

This controls the NPS Setting Current for the Active Protection/Detection group

3

1260

Amps

1

50—14.70

B.2

44

Broken Conductor Setting Current Active

This controls the Broken Conductor Setting Current for the Active Protection/Detection group

3

1260

Amps

1

50—14.70

B.2

45

Phase Setting Current Active

This controls the Phase Setting Current for the Active Protection/Detection group

3

1260

Amps

1

50—14.70

B.2

46

Earth Setting Current Active

This controls the Earth Setting Current for the Active Protection/Detection group

3

1260

Amps

1

50—14.70

B.2

47

SEF Setting Current Active

This controls the SEF Setting Current for the Active Protection/Detection group

3

1260

Amps

1

50—14.70

B.2

48

NPS Setting Current Active

This controls the NPS Setting Current for the Active Protection/Detection group

3

1260

Amps

1

50—14.70

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.