PKR39809-02

System Measurements

System Measurements are a condensed version of the full range of measurements available on the PowerLogic ADVC Controller. They provide a snapshot of the power system measurements in real time.

System Measurements display three phase values for power and PF but the current and voltage values are three phase averages.

System Measurements are displayed on the flexVUE and setVUE operator interfaces.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.