PKR39809-02

Additional System Status pages

Additional pages are added to the System Status display group when certain features are made available. When Plant Details is made available, that page appears following the Switchgear Wear/General Details page.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?