PKR39809-02

Lamp Reset

Pressing the Lamp reset key clears the status lamps. This forces the indicators to the logic false state. However, the status lamps are continuously updated and will change back to the logic true state if the conditions are still true.

Example: if the battery supply was OK prior to pressing the reset key, it will again indicate OK afterwards.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.