PKR39809-02

SOHIR

SOHIR offers an alternative to the traditional Zero-Detect method of Inrush Restraint explained in Inrush Restraint Operation.

High inrush current is often due to magnetizing current when a transformer is energized.

Magnetizing currents are distinguished by their high second order harmonic content. SOHIR provides rapid harmonic detection of inrush current based on harmonic content.

Making SOHIR Available

SOHIR is an optional feature and can be enabled on the Feature Selection page in WSOS.

Display > Configuration > Feature Selection > Detection

Or on the operator interface.

SOHIR Configuration

When SOHIR has been made available, an additional field, Inrush Restraint Type, is added to the Inrush Restraint settings. The setting options for this field are:

  • Zero Detect

  • SOHIR

Figure 203
Inrush Restraint Type Selection

Two more settings are added if SOHIR is selected as the Inrush Restraint type.

  • Inrush Restraint Threshold

  • Inrush Restraint Algorithm

Figure 204
SOHIR Inrush Restraint settings

SOHIR can also be selected and configured on the operator interface.

The parameters used to configure SOHIR Inrush Restraint are described in the table below:

Table 77 Inrush Restraint Settings

Setting

Default

Description

Inrush Restraint Time

0.10 s

The time Inrush Restraint will remain active when triggered.

Inrush Restraint Multiplier

X4

Setting current multiplier while Inrush Restraint is active.

Inrush Restraint Threshold

20%

The 2nd harmonic component of current on the line (expressed as a percentage of the fundamental component) required for SOHIR to activate.

Inrush Restraint Algorithm

AND

Configured for either AND or OR. In the case of AND logic, all phases must have harmonics above the threshold setting, in order for SOHIR to become active. In the case of OR logic, only the phase with the highest current needs to have harmonics above the threshold setting.

SOHIR is configured per detection group.

SOHIR Operation

SOHIR monitors pickups by either Phase, Earth or NPS protection elements.

  • Once a pickup is detected, SOHIR restrains all overcurrent protection trips from the Phase, Earth or NPS elements (except those using Definite Time curves) for 30 ms.

  • During this 30 ms time period, SOHIR calculates the harmonics on the faulted phases as a percentage of the fundamental component.

  • If one or more phases has a second harmonic component above the Inrush Restraint Threshold setting, a decision is made on whether to become active based on the Inrush Restraint Algorithm.

  • If SOHIR does become active it will restrain all overcurrent trips from the Phase, Earth and NPS element for the configured Inrush Restraint Time.

SOHIR will be deactivated if either:

  • Harmonics measured during the 30 ms period are below the threshold.

  • The Inrush Restraint timer has expired.

Once SOHIR has been deactivated it cannot reactivate until all relevant protection elements have reset.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.