PKR39809-02

Appendix G ­ Reset Curve Timing Tables

Reset times (T) for IEEE Reset Curves can be calculated using the following formula.

IEEE Moderately Inverse

T= 4.85* Time Multiplier / (M² - 1)

IEEE Very Inverse

T= 21.6* Time Multiplier / (M² - 1)

IEEE Extremely Inverse

T= 29.1* Time Multiplier / (M² - 1)

If the Reset Curve starting point is set to Reset Threshold,

M = (Measured Current) / (Reset Threshold x Pickup Current).

If the Reset Curve starting point is set to Pickup,

M = (Measured Current) / (Pickup Current).

Tables listing the reset times in seconds for IEEE Reset Curves are given below.

Table 111 IEEE Reset Curves Timing Table

% of Setting Current

IEEE Inverse

IEEE Very Inverse

IEEE Extremely Inverse

0%

4.85

21.60

29.10

5%

4.86

21.65

29.17

10%

4.90

21.82

29.39

15%

4.96

22.10

29.77

20%

5.05

22.50

30.31

25%

5.17

23.04

31.04

30%

5.33

23.74

31.98

35%

5.53

24.62

33.16

40%

5.77

25.71

34.64

45%

6.08

27.08

36.49

50&

6.47

28.80

38.80

55%

6.95

30.97

41.72

60%

7.58

33.75

45.47

65%

8.40

37.40

50.39

70%

9.51

42.35

57.06

75%

11.09

49.37

66.51

80%

13.47

60.00

80.83

85%

17.48

77.84

104.86

90%

25.53

113.68

153.16

95%

49.74

221.54

298.46

99%

243.72

1085.43

1462.31

Reset times (I) for IEC 255 Reset Curves can be calculated using the following formula.

IEC 255 Inverse

T= 13.5* Time Multiplier / (M² - 1)

IEC 255 Very Inverse

T= 47.3* Time Multiplier / (M² - 1)

IEC 255 Extremely Inverse

T= 80* Time Multiplier / (M² - 1)

If the Reset Curve starting point is set to Reset Threshold,

M = (Measured Current) / (Reset Threshold x Pickup Current).

If the Reset Curve starting point is set to Pickup,

M = (Measured Current)/(Pickup Current)

Tables listing the reset times in seconds for IEC 255 Reset Curves are given below.

Table 112 IEC 255 Reset Curves Timing Table

% of Setting Current

IEC 255 Inverse

IEC 255 Very Inverse

IEC 255 Extremely Inverse

0%

13.50

47.30

80.00

5%

13.53

47.42

80.20

10%

13.64

47.78

80.81

15%

13.81

48.39

81.84

20%

14.06

49.27

83.33

25%

14.40

50.45

85.33

30%

14.84

51.98

87.91

35%

15.38

53.90

91.17

40%

16.07

56.31

95.24

45%

16.93

59.31

100.31

50&

18.00

63.07

106.67

55%

19.35

67.81

114.70

60%

21.09

73.91

125.00

65%

23.38

81.90

138.53

70%

26.47

92.75

156.86

75%

30.86

108.11

182.86

80%

37.50

131.39

222.22

85%

48.65

170.45

288.29

90%

71.05

248.95

421.05

95%

138.46

485.13

820.51

99%

678.39

2376.88

4020.10

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.