PKR39809-02

Symbols

The following symbols are used to identify the circuit breakers on the PSM.

Symbol Description

AC Supply (115 or 230 Vac)

General Purpose Outlet (GPO) (Optional)

Battery

Second 115 or 230 VA AC Supply (Optional)

Integrated Supply Voltage Transformer (VT) (Optional)

NOTE: It is possible to have 2 AC supplies and an Integrated supply fitted in the same unit.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.