PKR39809-02

Appendix K.9 ­ setVUE AS Detection Menu Pages

This appendix lists all of the Detection display group pages.

The basic Detection display group consists of 15 default pages.

Up to 23 additional pages and 5 alternate pages can be added to the detection menu depending on the features that have been enabled.

The table below shows the complete list of available pages and their position in the Detection menu.

Table 148 setVUE Detection Menu Pages

Detection Menu

Default Pages

Additional Pages

Alternate Pages

Detection Setting 1

   

Detection Setting 2

   

Detection Setting 3

   

Detection Setting 4

   

Detection Setting 5

   
 

Detection Setting Alarms 1(1),(2)

 
 

Detection Setting Alarms 2(1),(2)

 
 

Detection Setting Extended(2)

 

Detection Setting 6

   

Cold Load Pickup Detection

   
 

Sync Check Settings 1(3)

 
 

Sync Check Settings 2(3)

 
 

Sync Check Settings 3(3)

 
 

Sync Check Settings 4(3)

 
 

Broken Conductor(4)

 
 

Directional Detection Phase 1(5)

Directional Blocking – Phase 1(6)

 

Directional Detection Phase 2(6)

Directional Blocking – Phase 2(5)

 

Directional Detection Earth 3(6)

Directional Blocking – Earth 3(5)

 

Directional Detection Earth 4(6)

 
 

Directional Detection SEF 5(6)

Directional Blocking – SEF 5(5)

 

Directional Detection SEF 6(6)

 
 

Directional Detection NPS 7(6)

Directional Blocking – NPS 7(5)

 

Directional Detection NPS 8(6)

 
 

VZPS Compensation(5)

 
 

High VZPS Alarm(5)

 
 

Under Voltage Detection(7)

 
 

Over Voltage Detection(7)

 
 

Under/Over Voltage Detection(8)

 

Phase Detection

   

Phase Single Shot Det Trip

   

Earth Detection

   

Earth Single Shot Det Trip

   

SEF Detection

   

SEF Single Shot Det Trip

   

NPS Detection

   

NPS Single Shot Det Trip

   
 

Fault Locator(9)

 
 

Conductor Characteristics(8)

 

(1) Per Element Detection available

(2) Extended Standard Detection On

(3) Sync Check available

(4) Broken Conductor available

(5) Directional Detection On

(6) Directional Blocking On

(7) Under/Over Voltage Detection available

(8) Under/Over Voltage Detection available

(9) Fault Locator available

The top line of each page is the page title. To the right of the title is the letter D which indicates that the page being displayed is part of the Detection display group.

The next three lines are the data or information on display. Most displays have six data fields. The standard layout is shown below.

If the standard menu is running, the Detection menu can be accessed by pressing the Panel On key and then pressing the Menu key three times.

The first page to be displayed in the Protection menu is the Protection Settings 1 page shown below.

Detection Settings 1

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.