PKR39809-02

Connect the IOEX to the Controller

Connect the IOEX power supply lead to the terminals on the side accessory tray. The terminals are marked with the following symbols.

Figure 319
IOEX Power Supply connection

Using the RS232 cable (ADC-640), connect the IOEX to a RS232 port on the PowerLogic ADVC Controller.

The options are:

  • PowerLogic ADVC

    • IOEX/WSOS port,

    • USB 1, 2, or 3 via a USB/RS232 converter.

Before the IOEX can be used it must be made available in the WSOS Feature Selection tool and assigned a communications port. It may also be necessary to configure and download a custom mapping file.

Please see: IOEX Configuration Tool.

Figure 320
IOEX Communications connection

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.