PKR39809-02

Default Configuration

The QAKs are programed in the factory to a default configuration but can be changed to suit operational requirements. WSOS includes a tool to modify the logic function and lamp for each QAK and a utility to print new labels. Refer to flexVUE customisation for more information.

The default configuration has been chosen to provide access to frequently used actions and is shown below:

Figure 17
flexVUE O.I. Default QAKs

The table below describes the function of each of the default QAKs. Pressing each key causes its Action which is confirmed by its LED changing to the Color shown.

Table 4 flexVUE O.I. default QAK descriptions

QAK ID Color Description Action
Column D

d-1

Red

Live Load Blocking

Toggles the Live Load Blocking feature ON/OFF.

d-2

Red

Loop Automation

Toggles the Loop Automation feature ON/OFF.

d-3

Red

Battery Test

Performs a Battery Test.

d-4

Red

Group A Protection

Protection Group A becomes Active.

Column E

e-1

Red

Auto ACR/LBS

Toggles Auto Reclose ON/OFF (for ACRs) or Sectionalise Auto/Off (for ASs).

e-2

Red

Ground Fault

Toggles Earth (Ground) Fault protection ON/OFF.

e-3

Red

Sensitive Ground

Toggles Sensitive Earth (Ground) Fault protection ON/OFF. (Providing Ground Fault is ON)

e-4

Red

Group B Protection

Protection Group B becomes Active.

Column F

f-1

Red

Turns REMOTE control ON (and LOCAL control OFF).

Turns REMOTE control ON (and LOCAL control OFF).

f-2

Red

Turns LOCAL control ON (and REMOTE control OFF).

Turns LOCAL control ON (and REMOTE control OFF).

f-3

Red

Toggles Hot Line Tag (Work Tag) Applied/OFF.

Toggles Hot Line Tag (Work Tag) Applied/OFF.

f-4

Red

Protection Group C becomes Active.

Protection Group C becomes Active.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.