PKR39809-02

Intelligent LA Communications

When LA is configured for Intelligent logic, each device requires its communications parameters to be configured.

In WSOS the LA Communications page can be opened by going to:

Display > LA > Communications.

The parameters to be configured will depend on the device type and tie control. Communications parameters for Feeder and Mid-Point devices will also differ according to the downstream device type.

Figure 238
Intelligent LA Communications for a Feeder with Mid-Point and Tie downstream devices and Message Tie Control

Figure 239
Intelligent LA Communications for a Feeder with Mid-Point and Tie downstream devices and Timer Tie Control

Figure 240
Intelligent LA Communications for a Mid-Point with Mid-Point and Tie downstream devices and Message Tie Control

Figure 241
Intelligent LA Communications for a Mid-Point with Mid-Point and Tie downstream devices and Timer Tie Control

Figure 242
Intelligent LA Communications for a Tie with Message or Timer Tie Control

Intelligent LA communications parameters can also be configured on the operator interface.

For a description of the settings on these pages, see Intelligent LA Communications Parameters.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.