PKR39809-02

Radio

Radio

Radio Supply OFF

Radio Supply ON

Radio Supply Shutdown

D

Radio Supply 12 V

(Range 5 V...15 V)

P

Radio Hold Time 60 min

(Range 0 min...1440 min)

P

Switchgear Type and Ratings displays information about the connected switchgear. The controller reads this information from the SCEM.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.