PKR39809-02

Plant Name

When the O.I. is activated, the Start Up screen is displayed briefly. The text Intelligent Power which appears by default, can be replaced by a user defined 20 characters message or Plant Name. The purpose of the Plant Name is to help operators identify the plant that they might be planning to operate.

The text required to be displayed by the O.I. on start-up can be entered in the Plant Name field on the WSOS Status page.

he Plant Name field on the WSOS Status page will accept 90 characters but only the first 20 are displayed on the O.I.

Changing the Plant Name will generate a record in the Event Log.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.