PKR39809-02

System Properties

WSOS System Properties can be opened in WSOS by selecting Properties in the Customise menu.

The System Properties contains the following pages:

  • Directories: Includes information on where directories associated with WSOS are located.

  • Mail: Contains the Mail Profile used when emailing Switchgear files and in the reporting of WSOS issues to Schneider Electric.

  • Log: Logging provides diagnostic support for WSOS to help Schneider Electric to make sure that WSOS is running as it must.

  • Start up: The Start Up page specifies which of the Launch Pad pages to load when WSOS starts up, or whether to show the Launch Pad at all.

  • Colors: The Colors Page allows you to customize the color of the text and its background for special fields in WSOS.

  • Advanced: The Advanced page contains customizable user interface options for WSOS.

  • Upgrade: The Upgrade page contains options on how to handle different WSOS switchgear file versions.

  • Convert: The Convert page contains an option to convert all the WSOS4 version files to WSOS5 version files.

  • Fonts: The Fonts page contains an option to change the font of the switchgear explorer and other tree control fonts.

  • Dots per inch: The dots per inch page contains an option to change the dots per inch displayed on the screen.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.