PKR39809-02

IEC 60870-5-101

There is a five-step procedure required to enable the PowerLogic ADVC Controller to communicate with a SCADA master station using the
IEC 60870-5-101 protocol:

  1. Check that IEC 60870-5-101 is available.

  2. Select a communications port for IEC 60870-5-101.

  3. Configure the communications settings for the selected port.

  4. Assign the selected port to IEC 60870-5-101.

  5. Configure the IEC 60870-5-101 settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.