PKR39809-02

Step 1 - Check that IEC 60870-5-101 is Available

The IEC 60870-5-101 communications protocol is included in all PowerLogic ADVC Controller firmware releases but before it can be configured or assigned to a communications port it may need to be made available. This can be done through Feature Selection in WSOS at:

Display > Configuration > Feature Selection > Communications

IEC 60870-5-101 can also be made available via the operator interface.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.