PKR39809-02

Cubicle Options

The PowerLogic ADVC Controller Range is available with either of two cubicles, the ultra and the smaller compact version.

Both cubicles are the same depth but the Ultra is taller and slightly wider. Both cubicles are fitted with the same vandal resistant door handle, although the ultra utilizes three point locking and the compact has a two-point locking system. Both cubicles are fitted with the same door stay mechanism which helps to secure the door open at 135°. The extra room in the ultra cubicle means that it can house an additional equipment tray whereas the compact only has room for one.

Both ultra and compact cubicles can be fitted with either of the optional O.I. that is setVUE or flexVUE.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.