PKR39809-02

GFN Operation

GFN is asserted for a network ground/EF when each of the following criteria are met:

  1. Zero Sequence Voltage (V0) magnitude is greater than or equal to a user defined GFN threshold setting.

  2. Phase-Earth voltages on two phases are above a user defined GFN uplifted phase voltage threshold setting.

  3. Phase-Earth voltage on one phase is less than a user defined GFN faulted phase voltage threshold setting.

The following functions of the ACR are disabled when GFN is asserted:

  • EF protection

  • SEF protection

  • Automatic Reclose

On clearance of a ground/EF and when GFN resets, the following ACR functions are in immediate effect:

  • EF protection

  • SEF protection

  • Start of user configured Auto Reclose block time

  • Inhibit of Auto Reclose function until the user configured block time expires

A recurrence of a ground/EF that causes GFN to be asserted before the expiry of the Auto Reclose Block time will result in:

  • EF protection disabled

  • SEF protection disabled

  • Auto Reclose functionality disabled and the Auto Reclose Block timer reset to the user configured value

A recurrence of a ground/EF that causes GFN to be asserted after the expiry of the Auto Reclose Block time will result in:

  • EF protection disabled

  • SEF protection disabled

  • Auto Reclose functionality disabled

Table 46 GFN Settings/Specifications

GFN Settings/Specifications

Setting

Minimum Value

Maximum Value

V0 Pickup Threshold

V0 Reset Threshold setting + 0.02 pu

2.00 pu

V0 Reset Threshold

0.00 pu

V0 Pickup Threshold – 0.02 pu

Auto Reclose Block Time

0 s

3600 s

Uplifted Phase Pickup Threshold

Uplifted Phase Reset Threshold setting + 0.02 pu

2.00 pu

Uplifted Phase Reset Threshold

0.00 pu

Uplifted Phase Pickup Threshold – 0.02 pu

Faulted Phase Pickup Threshold

0.00 pu

Faulted Phase Reset Threshold setting – 0.02 pu

Faulted Phase Reset Threshold

Faulted Phase Pickup Threshold setting + 0.02 pu

2.00 pu

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.